Skip to main content
Visitor II
November 14, 2016
Question

LIS2DH12 data ready interrupt

  • November 14, 2016
  • 1 reply
  • 627 views
Posted on November 14, 2016 at 07:37

Hi,

I want the most basic function -- data ready interrupt, but it seems not so easy to come out. Here are my configurations:

void lis3dh_init(void)

{

  //Inizialize MEMS Sensor

lis3dh_reset();

  //set ODR (turn ON device)

  LIS3DH_SetODR(LIS3DH_ODR_50Hz);

  //set PowerMode 

  LIS3DH_SetMode(LIS3DH_NORMAL);

  //set Fullscale

  LIS3DH_SetFullScale(LIS3DH_FULLSCALE_4);

  //set axis Enable

  LIS3DH_SetAxis(LIS3DH_X_ENABLE | LIS3DH_Y_ENABLE | LIS3DH_Z_ENABLE);

LIS3DH_SetInt1Pin(LIS3DH_CLICK_ON_PIN_INT1_DISABLE | LIS3DH_I1_INT1_ON_PIN_INT1_DISABLE |

LIS3DH_I1_INT2_ON_PIN_INT1_DISABLE | LIS3DH_I1_DRDY1_ON_INT1_ENABLE | LIS3DH_I1_DRDY2_ON_INT1_DISABLE |

LIS3DH_WTM_ON_INT1_DISABLE | LIS3DH_INT1_OVERRUN_DISABLE   );

//initialize the pedometer 

IntPedomter();

}

void get_acc_data(void)

{

if(!g_int_triggered) return;

AxesRaw_t data;

LIS3DH_GetAccAxesRaw(&data);/* Read the accel XYZ data*/

PEDO_SampWrite(((data.AXIS_X)>>6)<<3, ((data.AXIS_Y)>>6)<<3, ((data.AXIS_Z)>>6)<<3);

// PRINTF(''%d\t%d\t%d\n'', (data.AXIS_X)/8, (data.AXIS_Y)/8, (data.AXIS_Z)/8);

}

And I've already configure the INT1 pin as a low-to-high edge triggered pin. But when I use the oscilloscope to get the waveforms, it is a straight line, I cannot see any change from it. And also cannot get any acceleration data.

So my question is how to configure the data ready interrupt correctly? Thank you.
    This topic has been closed for replies.

    1 reply

    ST Employee
    November 30, 2016
    Posted on November 30, 2016 at 14:12

    I think the sensor is not running (it is in power down mode), because you don

    ’

    t get any data.

    In consequence data ready interrupt can not occur.

    In principle you configuration is correct, but I don

    ’t know what is going on in your functions LIS3DH_SetXxxx(…)

    .

    To enable data ready interrupt on INT1 pin, you have to set bit I1_DRDY1 in CTRL_REG3(0x22h).

    Best regards

    Miroslav