LIS2DH12: Interrupt issue with click configuration
Hi everyone,
For my application I used the LIS2DH12 MEMS in single click configuration. This is my setting:
CTRL_REG1 = 0x5F // ODR=100Hz, Low Power mode, Z Y X axis enable
CTRL_REG4 = 0x00 // Full Scale(FS):+/- 2G, high resolution disable (low power mode)CTRL_REG6 = 0x82 // Click interrupt on INT2 pin, interrupt active lowCLICK_CFG = 0x15 // Enable interrupt single-click on X-axis, Y-axis and Z-axis CLICK_THS = 0x0D // Click threshold: LSB=FS/128 -> Threshold = CLICK_THS*LSB = 0.2G CLICK_TIME_LIMIT = 0x02 // Time limit: LSB = 1/ODR -> Interval = CLICK_TIME_LIMIT*LSB = 20msCLICK_TIME_LATENCY = 0x64 // Time latency = 100msMEMS works fine, with a good click sensitivity in every direction, but there is a issue....
When I move the MEMS slowly, there is some position that the interrupt remains low. It return high only if I move the MEMS again.
Why this happens? Is it the setting too much sensible?
Thank you for your help.....
#lis2dh12