Skip to main content
Visitor II
October 29, 2018
Solved

LIS2DH12: problem while measuring degree of inclination in 0 - 360 values

  • October 29, 2018
  • 6 replies
  • 1936 views

Hello there,

I have a device called RuuviTag that includes your LIS2DH12 accelerometer and that can be programmed by means of an IDE called Espruino in JavaScript.

For a project, I am trying to get the tilt angle of the device measured in degrees with a value between 0 and 360. At the moment, however, I'm not succeeding and looking on the internet I found this documentation:

https://www.st.com/content/ccc/resource/technical/document/application_note/d2/d6/22/4f/b9/8f/45/59/DM00119046.pdf/files/DM00119046.pdf/jcr:content/translations/en.DM00119046.pdf

Do you have any code to which I can get information for this problem? I tried to use equation 2 but it doesn't give me back the angle. I also tried equation 6 but it doesn't work. 

The values I can take from the accelerometer are values in mg.

Here is the photo:

0690X000006CH1aQAG.png

Do you know how to help me?

Thanks.

    This topic has been closed for replies.
    Best answer by Miroslav BATEK

    These formulas works for range -90° to +90° in all three angles:

    0690X000006CH53QAG.png

    For Pitch you can use other formula for range -180° to + 180°:

    Pitch = arctan2 (Y/Z)

    6 replies

    ST Employee
    October 29, 2018

    These formulas works for range -90° to +90° in all three angles:

    0690X000006CH53QAG.png

    For Pitch you can use other formula for range -180° to + 180°:

    Pitch = arctan2 (Y/Z)

    danybrAuthor
    Visitor II
    October 29, 2018

    Hi Miroslav, thank you very much.. It seems to be working properly!

    In order to make that I used:

    pitch = (((Math.atan2(accelerationY,accelerationZ) * 180) / 3.14 ) + 180 );

    By using the AccelerationY and accelerationZ provided by the device, than converted in degree and "+180" offset to get values from 0 to 360.

    danybrAuthor
    Visitor II
    December 9, 2018

    Hi @Miroslav BATEK​ 

    I have a fairly serious problem: I hadn't considered angular acceleration!

    In summary: the device that integrates the LIS2DH12 sensor reads the data with a frequency of 100 hz, for each sample from sensor (Ax,Ay,Az) it calculates the pitch and when a revolution (round/lap) is completed (so when the samples pass in sequence between 0-90°, then 90°-180°, then 180°-270° and finally 270°-360°) the counter is increased.

    Calculating the pitch with the formula you gave me works, but only for tests made with the device moved by hand.

    In fact, the device is now mounted on the crankshaft of a rotating motor and the device has to measure its revolutions. Now, after a certain rotation speed, the device is no longer able to measure these revolutions because (I suppose) it can no longer calculate the pitch correctly.

    I absolutely need to find a way to count the number of revolutions made by the engine by means of this device. Do you have any suggestions? I would like to continue on the path of calculating pitch, but if it is not possible I am open to other ways, just include this sensor (I do not have the ability to add additional hardware).

    Thank you very much!

    ST Employee
    December 10, 2018

    I suppose the accelerometer is saturated by centrifugal force, so the only solution is to place the accelerometer to the center of the shaft. It would be good to see the acceleration data comming from the sensor in real situation. The you can evaluate if there is other option how to calculate the number of revolution.

    I think it is not good idea to measure the number of revolution by accelerometer, using optical or magnetic sensor would be much easier.

    danybrAuthor
    Visitor II
    January 3, 2019

    Hi @Miroslav BATEK​,

    I'm trying to get more information about problem that I have, in order to find a solution.

    In a static situation, angle of inclination (pitch in this case) is calculated right. Could you explain please the math behind this calculus? Why it works? Specifically, I did not quite understand how the accelerometer values are turned into an angle. I know the interpretation of the atan2 function, but I do not understand how the vectors detected by the sensor are then interpreted in a goniometric circumference and turned into an angle. I can not base myself on what I read in your datasheet:

    https://www.st.com/content/ccc/resource/technical/document/application_note/d2/d6/22/4f/b9/8f/45/59/DM00119046.pdf/files/DM00119046.pdf/jcr:content/translations/en.DM00119046.pdf

    For example, I get a pitch of 103,94 if I get values y: -0,980 and z: 0,244 with accelerometer with a face towards me, so:

    0690X000006CxQQQA0.png

    Thanks!

    ST Employee
    January 6, 2019

    I'm sorry, but I can't explain here the basic principles.

    I recommend you ask some of you colleague with a good physics knowledge.