LIS2DH12 Z-axis value is reported with the opposite sign
Hi,
I've been working with the LIS2DH12 sensor for quite some time, primarily utilizing the X and Y axes without any issues. However, for a new project, I also need to incorporate the Z-axis. I've noticed that while the acceleration values reported are accurate, in terms of absolute value, the sign is the opposite than expected.
Is this a bug already known? I haven't found any ticket or post talking about it, and it seems strange to me.
I am expecting the following axis reference.

Every time I put the sensor oriented with the X or Y axis pointing down (totally vertical), I get +1g acceleration, but if do the same with the Z-Axis, I get -1g acceleration.
Could any one help me?
Thank you in advance.
Regards,
Luis