Skip to main content
Visitor II
November 22, 2019
Question

LIS2DS12 Direction of the accelerations?

  • November 22, 2019
  • 1 reply
  • 569 views

Use 3-axis acceleration LIS2DS12

page 10 figure 2 Pin description in datasheet

The z direction is reversed in the output, but I don't know why.

ex) Gravity acceleration is displayed as + g.

    This topic has been closed for replies.

    1 reply

    ST Employee
    November 25, 2019

    Hi @Jlee.1572​ , the reading is correct. The accelerometer sense the 1g gravity acceleration but in the direction of the reaction constraint exercised by the surface on which you have placed the device (so, bottom-up direction). To understand this, please note that in case you left your device fall (free fall condition), the sensed acceleration will reduce to 0g. Regards