Question
LIS2DS12 needs I2C pull up or not?
I am using STEVAL-MKI174V1 adapter board for LIS2DS12 evaluation. I checked the schematic of STEVAL-MKI174V1 and I have two questions:
- Can Vdd for STEVAL-MKI174V1 be 3.3V without damaging LIS2DS12 because it can handle only 2.2V (It seems answer to this will be yes because of regulator)
- Do I need to add external pull-ups to SDA, SCL line even after adapter board ?
Thanks,
Kiran