LIS2DTW12 Aliasing cut off
Hello,
I'm using an LIS2DTW12 and I don't understand very well which is the cut off frequency.
I'm quite confused because from this picture seems that the anti aliasing filter has cut off frequency fixed to 400 Hz :
Then in this table the cut off frequency after the LPF1 and LPF2 seems ODR/2:
I'm interested in the 0-100Hz part of the acceleration so my ODR is 200 Hz.
I want know if the part of the acceleration above 100Hz is cut off or if only the part above 400Hz is cut and then there will be aliasing.
Regards,
Riccardo