LIS2DW12, how are the interrupt pins internally connected?
LIS2DW12, if interrupt pins (INT1 & INT2) are configured to open-drain mode, will they still work if the VDDIO supply is cutoff? (and the interrupt pins are pulled up to another supply voltage) and the VDD is still connected to 1,8V ? Will the VDD voltage still control the open-drain pins or is it completely fed by the VDDIO voltage?
#lis2dw12