Question
LIS2DW12 ODR clock accuracy
Hello,
We have integrated LIS2DW12 sensor in our application and configured it as per below configuration,
- Mode: High performance mode
- ODR = 200Hz
- Sensitivity +/-2g
- FIFO with 32 samples
- INT2 interrupt for FIFO full
Our application requires 1% accuracy for sampling of the data. So I have below questions,
- What is ODR clock accuracy?
- How to measure ODR clock accuracy? Like measuring FIFO interrupt durations?
- If we want to perform sampling in application as per DT0102, sensor needs to be configured for ODR 50. Does someone knows whether we can use higher ODR setting of 200Hz in single conversion mode?
Thanks
Shri