Skip to main content
Visitor II
September 27, 2022
Solved

LIS2DW12 reserved pin functionality

  • September 27, 2022
  • 1 reply
  • 812 views

Hi,

I am debugging my custom board where I soldered an LIS2DW12 accelerometer on it. I forgot to pull the reserved pin ( 7 ) to ground as suggested in the datasheet.

This is how I connected it:

0693W00000SwLo5QAF.pngThis is how it should be connected:

0693W00000SwLoKQAV.pngIs this required, that the accelerometer can work properly? I cant find it on my I2C bus and don't know if it is related to this little mistake or maybe another, most likely soldering issue.

Edit: I2C is pulled up and decoupling capacitors are also there. Just on another section.

Thank you

    This topic has been closed for replies.
    Best answer by Eleon BORLINI

    Hi @CMoeb.1​ ,

    Yes, as stated in the datasheet, the RES pin has to be tied to GND... you might try to change the Vdd / VddIO level if you can, for example decreasing it to 1.8V (the pin should be less sensitive to lower voltages).

    -Eleon

    1 reply

    ST Employee
    September 28, 2022

    Hi @CMoeb.1​ ,

    Yes, as stated in the datasheet, the RES pin has to be tied to GND... you might try to change the Vdd / VddIO level if you can, for example decreasing it to 1.8V (the pin should be less sensitive to lower voltages).

    -Eleon