LIS2DW12 wake up interrupt or double-tap interrupt on INT2 pin
Hello all,
I am using LIS2DW12 accelerometer for single-tap and double-tap detection. I also want to use the wake-up interrupt simultaneously, but when both these interrupts are enabled, double-tap and single-tap are occasionally missed because both the wake-up interrupt and tap interrupts are routed to the same pin(INT1) and the wake-up threshold is low.
Is there any way in which I can route either the tap interrupt or the wake up interrupt to INT2 pin ?
I am aware that we can route INT2 interrupts to INT1 but can it be done the other way around?
Thank You