Question
LIS2HH12 Works for a moment and then stops working, value of 0 is being returned.(Using Arduino on a custom atmel328p board)

We have been using the LIS2HH12 accelerometer and it will work on a fresh board for about a day or so and then stop working. Below is some stripped down code from this library:
https://gitlab.com/rhombio/rhio-libraries/rhio-LIS2HH12/-/blob/master/examples/basic-example.cpp
#include <U8g2lib.h>
#include <Arduino.h>
#include <rhio-LIS2HH12.h>
float x, y, z;
char bufferx[80];
char buffer_display[80];
U8X8_SSD1306_128X32_UNIVISION_4W_SW_SPI u8x8(/* clock=*/ 13, /* data=*/ 11, /* cs=*/ 10, /* dc=*/ 8, /* reset=*/ 9);
LIS2HH12 lis = LIS2HH12();
void setup()
{
Serial.begin(9600);
lis.begin();
lis.setBasicConfig();
u8x8.begin(); //Set up OLED Display
u8x8.setPowerSave(0);
}
void loop()
{
lis.getAccel(&x, &y, &z);
sprintf(bufferx,"xAngle:%d",round(x));
delay(333); //333
u8x8.setFont(u8x8_font_8x13B_1x2_r); //Set Font for mode and angle
u8x8.draw1x2String(0,0,bufferx);
delay(2000);
}
#include <U8g2lib.h>
#include <Arduino.h>
#include <rhio-LIS2HH12.h>
float x, y, z;
char bufferx[80];
char buffer_display[80];
U8X8_SSD1306_128X32_UNIVISION_4W_SW_SPI u8x8(/* clock=*/ 13, /* data=*/ 11, /* cs=*/ 10, /* dc=*/ 8, /* reset=*/ 9);
LIS2HH12 lis = LIS2HH12();
void setup()
{
Serial.begin(9600);
lis.begin();
lis.setBasicConfig();
u8x8.begin(); //Set up OLED Display
u8x8.setPowerSave(0);
}
void loop()
{
lis.getAccel(&x, &y, &z);
sprintf(bufferx,"xAngle:%d",round(x));
delay(333); //333
u8x8.setFont(u8x8_font_8x13B_1x2_r); //Set Font for mode and angle
u8x8.draw1x2String(0,0,bufferx);
delay(2000);
}An oled display is being used as a serial monitor for this. Attached also are snippets from the schematic: