Question
LIS2MDL, MAGNETOMETER
Hello, I am using the LIS2MDL development kit. I have two questions.
- When I measure with two development kits in the same environment, I get different values.
Both are 5 cm away from each other and there is no factor that will disrupt the magnetic field around either of them.
What could be the reason for this? - When I bring a magnet closer to any of the development kits without changing its position and move it away, I get different measurements than the first values it measured.
For example:
x: 500 y: 100 z: 800
After moving the magnet closer and further away:
x: 200 y: -200 z: 450
When I reset the card nothing changes. It still reads the bad value. The position of the development kit does not change and I guarantee that the magnet is far enough away.
What is the reason for this?