LIS2MDL Magnetometer Compass Calculation - Left-Handed Coordinate System Issue
Hi,
We are implementing a compass application using the LIS2MDL magnetometer sensor and experiencing incorrect direction readings due to the sensor's left-handed coordinate system. The raw sensor data is functioning correctly, but standard compass calculation algorithms designed for right-handed coordinate systems produce inaccurate results.
Issue Summary:
- Sensor: LIS2MDL 3-axis magnetometer
- Problem: Compass calculations yield incorrect directions (primarily showing North/East instead of full 360° range)
- Root Cause: LIS2MDL uses left-handed coordinate system (confirmed from ST Community forum discussion)
- Impact: Standard compass algorithms fail to provide accurate bearings
Technical Details:
- Raw sensor readings are stable and changing correctly
- Sensor communication and initialization working properly (WHO_AM_I = 0x40)
- Sample raw data shows expected magnetic field variations
- Issue occurs during coordinate system conversion for compass heading calculations
Current Environment:
- Platform: Embedded Linux
- Interface: I2C
- Application: Digital compass/heading indicator
- Sensor Configuration: 100Hz ODR, continuous mode, BDU enabled
Datasheet refering to file:///C:/Users/raj82251/Downloads/LIS2MDL.PDF
I have refered some of the forum links https://community.st.com/t5/mems-sensors/lis2mdl-axis-directions/td-p/209018
Can you provide official documentation or application notes specifically addressing compass/heading calculations for LIS2MDL's left-handed coordinate system?
Please confirm the exact positive axis directions for LIS2MDL when mounted flat (PCB orientation) for compass applications.
What is the recommended mathematical transformation to convert LIS2MDL left-handed coordinates to standard compass bearings (0°=North, 90°=East, 180°=South, 270°=West)?
Do you have reference code or algorithms specifically for LIS2MDL compass applications that properly handle the left-handed coordinate system?
Are there any specific calibration procedures or offset corrections needed for compass applications with LIS2MDL?