LIS2MDL number of samples in low power mode Vs high resolution mode
Hi,
I'm looking for the information about the number of sensor ADC samples per output data, in low power mode Vs. the high resolution mode.
I found the following description in AN5069:
"The difference distinguishing the two modes is in the number of samples used to generate
each output sample, which is four times less in Low-Power mode than the number used in
High-Resolution mode, thus ensuring a lower power consumption"
However, I didn't found what the actual number is.
Thanks,
Dagan