Question
LIS331 return always zero when I read axis data
Posted on April 06, 2016 at 13:55
Hi everybody,
I use a LIS331 with I2C communication. I can read and write the configuration register (CTRL_REG1 for example) but when I want to read any data register, the read value is always zero. CTRL_REG1 value is 07h, therefore the axis are enabled. I have tried to read STATUS_REG and the value is zero. Anyone has had this problem ? Have I forgotten a step in configuration or something like that ? Thanks in advance. #lis331