LIS331HH self-test output change with voltage
We have performed the self test on two prototype boards,
as instructed in this post: https://community.st.com/s/question/0D50X00009XkXegSAF/lis331hh-understanding-self-test
The x and y differences are around 135, which is in the range, but on the z axis we get around 380, which according to the datasheet, is just enough to no pass the self test.
The datasheet also specifies that the "Self-test output changes with the power supply" and that the product was calibrated at 2.5V.
Our question is the following:
Can the fact that we use a different supply voltage (3.3V) be the reason why the self test (just barely) fails or does the range of the self test already account for potencial differences?
Best regards!