Skip to main content
Visitor II
December 1, 2017
Question

LIS3DE/H RES pin

  • December 1, 2017
  • 1 reply
  • 933 views
Posted on December 01, 2017 at 11:20

Hello,

I would like to ask what is 'RES' pin in LIS3DH and LIS3DE? The only informtion is that it should be connected to the ground. Is it hardware reset which is activated with high state?

    This topic has been closed for replies.

    1 reply

    Visitor II
    December 1, 2017
    Posted on December 01, 2017 at 17:00

    RES typically refers to RESERVED. However, this doesn't mean that the pin may not have a manufacturing purpose but that's not something I imagine they would share on a public forum......

    ST Employee
    December 1, 2017
    Posted on December 01, 2017 at 17:13

    Yes,

    Derbyshire.Aaron

    ‌ is right the pin is RESERVED and must be connected as it is stated in the datasheet. It is NOT reset pin.

    These pins might be used in production but are useless for end users.