Solved
LIS3DH: 12 Bit Resolution and FIFO Mode
Posted on November 30, 2017 at 11:19
Given that the LIS3DH FIFO is only 10 bit wide, is it actually possible to run the accelerometer with 12 bit resolution?
#12-bit #lis3dh #fifoGiven that the LIS3DH FIFO is only 10 bit wide, is it actually possible to run the accelerometer with 12 bit resolution?
#12-bit #lis3dh #fifoI think if the sensor is configured int Low-power mode (8-bit resolution) also only 8-bit value is stored in the FIFO (the low bytes are 0).
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.