Question
LIS3DH ADC Interrupt
Posted on May 17, 2018 at 12:06
Hello,
I
checked the lis3dh manual, there is such a sentence “
The status of the 321DA bit can be driven to the INT1 pad by setting the I1_DRY2 bit of CTRL_REG3 to 1.� ,I have do it(ADC_PD bit of TEMP_CFG_REG (1Fh) to 1,
ODR bit of CTRL_REG1(20h) to 1HZ ), but can’t get interruptes signals.INT1 pin is always high. other work well.
Thanks for your help.