LIS3DH ADC1 input troubleshooting
I've implemented a new low power design using LIS3DH, and I had in mind to use ADC1 input to monitor the battery voltage and ADC3 to monitor temperature.
I succeed to properly read all three accelerometers axis as well as temperature. On the ADC1 input if I connect directly a voltage controlled source I've got consistent measurment form about 0.8V up to 1.6V, but when I connect the resistor voltage divider (27MOhm pull up and 100MOhm pull down) with a divided voltage around 1.1V the measure clamp to -32768.
I did'nt succeed to find any information about ADC1 inpu impedance, behaviour our any application note.
The high impedance divider is setup to reduce standby current.
Any help would be gratefully appreciated.