Skip to main content
Visitor II
June 20, 2016
Question

LIS3DH Anti-aliasing

  • June 20, 2016
  • 1 reply
  • 1042 views
Posted on June 20, 2016 at 12:44

Does anyone have any characteristics for the AA filter and method on the LIS3DH accelerometer?

E.g. slope, number of poles, type...

Thanks

Kevin

#lis3dh
    This topic has been closed for replies.

    1 reply

    Visitor II
    May 11, 2017
    Posted on May 11, 2017 at 09:20

    Does anyone know something about the used anti-aliasing filter?

    Does the filter change if he ODR (Output Data Rate) is changed? The datasheet tells me YES.

    0690X00000606yLQAQ.png

    measured 19.8 Hz with the 100 Hz ODR.

    The anti-aliasing filter doesn't work as required. It should block frequencies above 50 Hz.

    The correct frequency is marked red below (sweep from 14 Hz to 19.8 Hz, later constant 19.8 Hz):

    0690X00000606yHQAQ.png

    Are there informations concerning the characteristic of the anti-aliasing filter?

    If the filter is always the same (setup for the fastest data rate), then the lower ODR are not useful.

    Do I have to use much higher data rates for measuring 19.8 Hz without errors from aliasing? 

    Visitor II
    May 18, 2017
    Posted on May 18, 2017 at 23:28

    Any news on the anti-aliasing filter characteristics?