LIS3DH configuration setting for INT2
I have seen that this query has been asked previously but there was no answer to it.
Therefore, I am raising the issue again here as follows:
Currently, I am using INT1 for free fall detection which is already outlined in the AN3308 application note. Together with this, I would like to use INT2 pin for shock detection.
So my question is what would be the sequence of settings to correctly configure LIS3DH INT2 for doing so. For shock detection, the idea is to do an interrupt where X || Y || Z (Logical OR) have a large acceleration signal for a certain amount of time (let's say over 5 or 10s).
Some parameter values would be really helpful for starter.
Thanks....