Skip to main content
Visitor II
November 25, 2014
Question

LIS3DH Documentation Incomplete

  • November 25, 2014
  • 2 replies
  • 707 views
Posted on November 25, 2014 at 14:46

All:

Are there any plans to complete the description for CTRL_REG6?

All other control registers have two tables, one high level to show the bits in the register, and a second table to describe in detail the bits.

CTRL_REG6 has only one table.

I have Doc ID 17530 Rev 1, dated May 2010.

#lis3dh #lis3dh
    This topic has been closed for replies.

    2 replies

    tba10596Author
    Visitor II
    November 25, 2014
    Posted on November 25, 2014 at 18:07

    CTRL_REG3 - unclear on bit assignments

    The first table shows 7 bits and -- for eighth bit. Does that mean that I1_CLICK is the most significant bit?

    It also looks like STATUS_AUX is a duplicate of STATUS_REG, and the only thing different is that XDA is now 1DA, YDA is now 2DA, etc. Is the behavior of the second ADC the same with respect to status?

    Regards,

    Todd Anderson

    tba10596Author
    Visitor II
    December 8, 2014
    Posted on December 08, 2014 at 14:32

    It turns out that both CTRL_REG3 and CTRL_REG6 have full documentation provided in the application report AN33008, page 18, Doc ID 18198 Rev 1, dated January, 2011.