LIS3DH High Resolution Threshold
Hi Community,
I am using Lis3dh sensor in 50HZ ODR, High Pass filter enabled with cut-off frequency 0.1 HZ with full scale range 8G and FIFO is enabled and set FIFO-to-Stream Mode.
Case 1:
I get interrupts for small events Normal Mode(HR bit is not set) for the same threshold and when i see the x,y,z axis value is more than the threshold.
Case 2:
With HR Bit enabled , I am not getting the interrupt for the same small event for the same threshold which means that event didn't cross the threshold.
I am sure both time same events only happened.
As per Datasheet and Application note, that Output value only will be in 12-bit in High resolution mode.
Is there HR bit anyway related to do with Threshold?
Please help me .
Thanks,
Hari