Question
LIS3DH HW or SW reset
Posted on October 14, 2016 at 09:14
Hello,
Is there a way to manually reset the LIS3DH? In our application, VCC is coming up *very* slowly, inherent to the system. I have the suspicion that the LIS3DH occasionally does not boot correctly as it fails self-test after boot. Power-cycling it brings it back to normal. Memory reboot (CTRL5:BOOT = 1) does not help. We have a clean reset source which takes care of the reset of the system. Is there another way to control the LIS3DH reset? There is a pin called 'RES' to be tied to GND which could stand for 'RESET' (or 'RESERVED'...). Thanks, Norbert