Skip to main content
Visitor II
March 18, 2018
Question

LIS3DH low peak to peak values (for machine vibration)

  • March 18, 2018
  • 1 reply
  • 618 views
Posted on March 18, 2018 at 21:35

I am using a LIS3DH to measure a machine's vibration, I understand that mems accelerometers are not usually used for this application, but nevertheless, I set up the acc to High resolution mode which gives me a bandwidth of 150Hz. I have the LIS3DH set up and comparing its data with a piezo accelerometer that I have. I noticed that at low frequency (under 40Hz) peak to peak values of both accelerometers are very similar. but when I go over that (80-100 Hz) I start to see a drop in the LIS3DH p-p compared to the other one. Is the LIS3DH just not suitable for this application ?

#lis3dh-machine
    This topic has been closed for replies.

    1 reply

    ST Employee
    March 19, 2018
    Posted on March 19, 2018 at 15:04

    What is the difference between the LIS3DH and the piezo sensor?