LIS3DH - Motion and crash detection
Hello all
My goal is to use two INT pins to generate two interrupts in a device which will be used in a car. INT2 will be pulled when a crash of the car is detected and INT1 when the car moves.
Here is my init setting:
CTRL_REG1 = 0x27 //10Hz, normal power mode, ZXY enable
CTRL_REG2 = 0x01 // HP filter for INT1
CTRL_REG3 = 0x40 //IA1 enable
CTRL_REG4 = 0x90 //4g | BDU
CTRL_REG5 = 0x0A //latch on INT1 and INT2
CTRL_REG6 = 0x22 //active low & INT2 enable
INT2_THS = 0x6D //~3500mg
INT2_DURATION = 0x00 // 0.1*0s
INT2_CFG = 0x2A //OR, X,Y,Z higher than threshold
INT1_THS = 0x02 //
INT1_DURATION = 0x03 //
INT1_CFG = 0x2A //
Generally, the motion detection part works fine (thanks to Miroslav). I am concerned about the crash detection part.The threshold is quite high (I don't want it to interrupt on every bump on the road) but it still sometimes interrupts when no hight acceleration is applied. It is very rare but still occurs.
If you have any inputs to this I'll appreciate.