Skip to main content
Visitor II
May 20, 2025
Question

LIS3DH tilt angle and shock interrupts + ADC

  • May 20, 2025
  • 1 reply
  • 351 views

Hi,

 

First of all, I'm not proficient with embedded C, but I would appreciate any input from you that I could feed to ChatGPT. I've been trying to have the codes generated, but they simply would not produce what I wanted. So I have a LIS3DH IMU connected to the ESP32 via I2C. I want to know if it is possible to have the ESP32 in deep sleep mode while waiting for the INT pins from the IMU to wake it up. INT1 should detect a shock of, say, 1.5 G-force, and INT2 for a tilt angle beyond a threshold. Since the ESP32 is asleep and not continuously polling the IMU, will this be possible? If so, can you provide hints on how to implement this?

Secondly, I have connected an analog lux sensor to ADC3 of the IMU. I'm getting variations when probing it with a multimeter but it's not reflected on the raw ADC readings. I'm certain it's within the scale.

 

Thank you very much.

    This topic has been closed for replies.

    1 reply

    Visitor II
    May 20, 2025

    a