LIS3DH Z output noisy
I am trying to measure a machine's vibration using LIS3DH sensor.
I set the LIS3DH in low power mode and 5.376 kHz sampling frequency which outputs 8 bit output. I use spi to get the data from the sensor. I changed this raw output into �g' using the sensitivity value given in the datasheet.
My problem is: The sensor shows a fluctuation in its output of Z axis even when there is no vibration applied and the sensor is fitted on a horizontal surface. The range of this fluctuation is approximately from 0.6g to 1.2g. I have attached a image that shows such output. (X axis is time and Y axis is vibration in terms of g)
Can someone please help me to interpret why this is happening ? Is there a method to somehow remove this noise from the output ?
Please help.