LIS3DHH ODR variation
Digital output data rate (ODR) of LIS3DHH is given (typically) as 1.1kHz in the datasheet. Does it mean ODR is not fixed in one sensor or it is fixed in one particular sensor but there is an inter device variation ? In either case, I am confused how to use the sensor without knowing the exact data rate. For comparison, I looked at LIS2HH12 (and IIS2DH), and it has configurable ODR, and it does not mention this is typical or not, so I assume it means it is fixed. If I need a fixed ODR, am I looking at the wrong sensor (LIS3DHH), are some sensors like this and some sensors like LIS2HH12 have fixed (configurable or not) ODR ?