Skip to main content
Visitor II
December 12, 2013
Question

LIS3DSH - error offset

  • December 12, 2013
  • 1 reply
  • 523 views
Posted on December 12, 2013 at 18:48

hi,

I use LIS3DSH and a problem appear sometime at init, in fact we catch false value from chip (offset error on x axis).

Only offset is not correct (same offset value in case of pb).

SPI bus reading is correct , value come from chip.

Do you have any reason for that , may we use any control to indentify error ?

Thnaks in advance,

Regard,

    This topic has been closed for replies.

    1 reply

    Visitor II
    January 10, 2014
    Posted on January 10, 2014 at 14:09

    Hello Thierry,

    What is the value that you are reading for the initial offset value?

    If possible, could you please attach the section where you setup CTRL_REG2 (21h) and an image showing the measured values?

    Thank you,

    Thiago Reis