LIS3DSH Interrupt output pin INT1 in movement detection application not working properly ?
I have seen here on this forum few questions concerning the interrupt issues, so I have the same problem, none of these previous questions have brought the answer so I wonder will this ever even work?
I first copied the ST app note AN3393 page 75 Wake Up -application register values.
The problem is that the interrupt occur once and only once, the lenght is 50us and after this sensor doesn't do any interrupts. After unplugging - plugging the power I again get one interrupt and then nothing.
When I set the interrupt (INT_1) to work as Data-ready interrupt to INT1. I see the interrupts occur on sample rate and altering the sample rate interrupts change accordingly.
One person on previous threads suggested adding OUTC (0x88) to the state machine to update the interrupt pins !??! This however didn't have any influence.
Is this a known problem in this sensor or how to get around this ?
Thanks.