LIS3MDL connected to ISM330dhcx as external sensor is giving NACK after some hours of continous run.
i have a maaxboard that is connected (via i2c) to ism330dhcx. Magnetometer LIS3mdl is connected(via i2c) to ism330dhcx as an external sensor.
reading magnetometer in power mode = ultra-high mode.
data rate = default
single converstion mode we get a nack saying magnetometer is not responding after 2 hours continuous run.
changed the power mode = lowe power mode and kept remaining same.
now i get MASTER STATUS of ISM330DHCX give NACK after 12 or 15hours of continuous run.
this is the schematics..
please help.. i need to run it continously.