Skip to main content
Visitor II
October 4, 2023
Question

LIS3MDL noise and maximum accuracy

  • October 4, 2023
  • 1 reply
  • 1322 views

In my system that found the heading angle using the LIS3MDL sensor, the maximum error value was 3 degrees using the ellipsoid calibration method. Also, although I used the sensor in low noise mode, I saw that the data in Matlab graphics was very wavy and noisy.
What is the accuracy value of the LIS3MDL sensor? What should I expect the max and average values to be? And what can I do to reduce noise?
Thanks for your help

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    October 4, 2023

    Hi @arslanoglu ,

    What do you mean as very noisy? On which axis? From our datasheet the RMS noise should be 3.2 mGauss for X and Y axis and 4.1 mGauss for Z axis.

    The accuracy depends on which is your FS, you can find it in the datasheet too.

    If this helps you, please mark my answer as "Best Answer" by clicking on the "Accept as Solution" button, this can be helpful for Community users to find this solution faster.