Skip to main content
Visitor II
February 6, 2019
Solved

Lowest power mode for accelerometer application in STM32L4 ?

  • February 6, 2019
  • 3 replies
  • 2088 views

Hi, I wanna use the lowest power mode possible for my stm32l432kc. I want MCU to wakeup on accelerometer motion (which is possible since the accel generate interrupt on motion). I've read in MCU appnopte AN4621(page 13) that i2c is detected only in stop mode and that it generate a wakeup on i2c address detection (if I understand it correctly). But as I explained this is not what I want. I wonder if I can use shutdown or standby?

    This topic has been closed for replies.
    Best answer by After Forever

    It depends on the accelerometer model and your schematics. Can it remain powered on and working while the MCU is in standby/shutdown mode? Does it send its wakeup event as a simple IO rising/falling edge which can be simply connected to MCU's WakeUp pin, or does it use the I2C as you think? I don't think it uses I2C to send an event (I've never seen an accelerometer which is I2C master rather than slave).

    3 replies

    ST Employee
    February 6, 2019

    Hello Maryam,

    For further information about the STM32L4 power mode you can refer to this training online session :

    https://www.st.com/content/st_com/en/support/learning/stm32-education/stm32l4-online-training.html

    Best Regards,

    Mohamed Aymen.

    Visitor II
    February 7, 2019

    @Community member​  can you please advise?

    Visitor II
    February 7, 2019

    If your accelerometer can generate an IO event then use the WKUP pin to catch the event and wake up from the standby/shutdown mode.

    Read the reference manual (RM0394), sections 5.3.9 (Standby mode) and 5.3.10 (Shutdown mode).

    Visitor II
    February 7, 2019

    So you think that the accelerometer would be able to detect motion while the MCU is in shutdown/standby mode and wakeup the MCU? Because as I mentioned in the post and what I could understand is that the accel won't be able to work unless the MCU is at least in the stop2 mode.

    Visitor II
    February 7, 2019

    It depends on the accelerometer model and your schematics. Can it remain powered on and working while the MCU is in standby/shutdown mode? Does it send its wakeup event as a simple IO rising/falling edge which can be simply connected to MCU's WakeUp pin, or does it use the I2C as you think? I don't think it uses I2C to send an event (I've never seen an accelerometer which is I2C master rather than slave).