Skip to main content
Visitor II
October 1, 2019
Question

LPF order in stop band for LIS2DTW12 device

  • October 1, 2019
  • 2 replies
  • 752 views

The datasheet for the device does not state the order of the LPF filters in the stop band. Should I assume it's 20dB/Decade attenuation?

Thanks.

Anthony.

    This topic has been closed for replies.

    2 replies

    AMoulAuthor
    Visitor II
    October 1, 2019

    Attempting to answer my own question, presumably the applied low-pass filter is just a programmable m-point smoothing filter (so its motion frequency response is going to be terrible - sin(Mw)/Msin(w)). At least the samples will look smooth!

    ST Employee
    October 4, 2019

    Hi Antony, I unfortunately cannot share you the frequency response of the LPF in LIS2DTW12 (but are you referring to the one on the inertial data path or or the temperature path?) However please consider that if you want to optimize the data accuracy, you can work in HP mode applying the anti-aliasing filter (@400Hz). Regards

    0690X000009k25BQAQ.png