LPS22HB PLE interrupt not working
Hi
I am working with the LPS22HB eval board from ST and trying to generate an interrupt when the pressure drops suddenly. So according to the data sheet this would be a PLE event (2nd bit of 0x0B register)
Below are my register settings -
reg 0x10 - 0x50
reg 0x12 - 0x03
reg 0x0B - 0x0A
I set the threshold registers 0x0C and 0x0D to the current value of pressure reading. I would expect that the int pin to change state from low to high after creating an external low pressure event but there is no change. Even the interrupt flag IA or PL from reg 0x25 is not set.
Now to make sure I did not have a bad device, I set the LPS22HB for generating an interrupt for a high pressure event. So I set bit PHE (1st bit in 0x0B reg) and the interrupt IS generated when I create a high pressure event. So everything works fine for a high pressure event interrupt. PH and IA Flag in reg 0x25 is set.
reg 0x10 - 0x50
reg 0x12 - 0x03
reg 0x0B - 0x09
The pressure readings when I poll registers 0x28, 0x29, 0x30 are also correct. It is just the low pressure interrupt event the is not working.
Unfortunately my product needs this low pressure interrupt event the most and LPS22HB would be a no-go if this cannot be fixed.
This seems like a bug to me. Is there anyone from ST that could look into this?
Or is there anyone in this forum who got this working?