Skip to main content
Visitor II
July 7, 2016
Question

LPS25HB unexpected behavior when FIFO is active

  • July 7, 2016
  • 1 reply
  • 1057 views
Posted on July 07, 2016 at 13:26

I've encountered a problem with LPS25HB. I'm trying to get maximum precision from this barometer sensor

without taking into account power consumption.

I've setted up registers in this way and in this order:

CTRL_REG1 0x20 => 0b11000110; // Power on, 25Hz, BDU, reset zero

RES_CONF 0x10 => 0b00001111; // AVG-P 512, AVG-T 64

After reading documentation I've tried to enable also FIFO in mean mode to get a more precise reading, in this way

and in this order

:

FIFO_CTRL 0x2E => 0b11000011; // FIFO Mean mode, 4 moving average

CTRL_REG2 0x21 => 0b01000000; // FIFO Enable

 Conversion that I do from readings are:

 Pressure = ReadedPressure /  4096UL;

Temperature = 42.5 + (ReadedTemperature / 480UL);

Reading are ok if I just initialize CTRL_REG1 and RES_CONF, correct temperature and reasonable pressure readings. But if I try to activate FIFO_CTRL and CTRL_REG2 (in this order, first FIFO_CTRL and after CTRL_REG2 registers), with above bit setup, I

suddenly have very wrong readings from Temperature and less precise values output from pressure. Temperature readings are not only wrong but they act like pressure readings, like if I move my PCB board up and down Temperature increase/decrease and when steady I've an AVG reading of 42�C.

Since I'm applying this formula that require temperature:

0690X0000060MnfQAE.gif

I want to ask what's wrong with this registers and FIFO.

Also, since I want to use FIFO mean to get less noise from output, I want to ask if it does effectivly reduce noise. Since I've already setted maximum AVG 512 for pressure and 64 for temperature, FIFO mean perform another AVG that can be useful? (I can't tell by myself since I was unable to get FIFO work correctly)

Thank you.

#lps25h
    This topic has been closed for replies.

    1 reply

    Visitor II
    July 18, 2017
    Posted on July 18, 2017 at 16:56

    Hi,

    I get exactly the same behavior. Is there some compatibilty bugs using at same time oversampling and movering average ?

    Thanks,

    Nicolas

    Graduate II
    August 15, 2017
    Posted on August 15, 2017 at 14:54

    Probably you are reading pressure and temperature data with one single autoincrementing I2C sequence. Doing so also gave strange temperature data for me. Reading pressure in one i2c sequence and temperature in another seqence gave sensible data.

    Visitor II
    September 14, 2017
    Posted on September 14, 2017 at 15:49

    Hi,

    I am now reading the Pressure and temperature with 2 différents sequences, Pressure is good but temperature is always much much higher than expected.

    Here is my config file:

    uint8_t pres_lps25h_config( void )

    {

        uint8_t who = 0;

        uint8_t tmp = 0;

        uint16_t offset = 0;

        /* Check Who Am I */

        who = baro_sensor_read_reg(LPS25H_WHO_AM_I);

        /* Rest and Boot */

        // Reset chip and wait 1 ms (4usec from datasheet)

        tmp = LPS25HB_SWRESET;

        baro_sensor_write_reg( LPS25H_CTRL_REG2, tmp );

        DelayMs(1);

        // Boot Enable and wait 4 ms (2.2 from datasheet)

        tmp = LPS25HB_BOOT;

        baro_sensor_write_reg( LPS25H_CTRL_REG2, tmp );

        DelayMs(4);

        /* Configuration */

        // LPS25H_RES_CONF (10h) : Config resolution (max average)

        tmp = LPS25HB_P_RES_AVG_512 | LPS25HB_T_RES_AVG_64 ;

        baro_sensor_write_reg( LPS25H_RES_CONF, tmp );

        // LPS25H_CTRL_REG1 (20h) : Power ON and ODR 25 Hz

        tmp = LPS25HB_MODE_ACTIVE | LPS25HB_ODR_25Hz | LPS25HB_DIFF_DISABLE | LPS25HB_BDU_CONT;

        baro_sensor_write_reg( LPS25H_CTRL_REG1, tmp );

        // LPS25H_CTRL_REG2 (21h) : FIFO Enable

        tmp = LPS25HB_FIFO_ENABLE ;

        baro_sensor_write_reg( LPS25H_CTRL_REG2, tmp );

        // LPS25H_CTRL_REG3 (22h) : No interruption

        // LPS25H_CTRL_REG4 (23h) : No configuration for interruption

        // INTERRUPT_CFG (24h) : No configuration for interruption

        // INT_SOURCE (25h) : No source for interruption

        // LPS25H_FIFO_CTRL (2Eh) : FIFO Config

     tmp = LPS25HB_FIFO_FIFO_MEAN | LPS25HB_FIFO_WTM_32;

     //tmp = LPS25HB_FIFO_BYPASS;

        baro_sensor_write_reg( LPS25H_FIFO_CTRL, tmp );

    ♯ if 0

        // The pressure offset value is a 16-bit data that can be used to implement One-Point

        // Calibration (OPC) after soldering, This value is composed of RPDS_H (3Ah) and RPDS_L

        // (39h). The value is expressed as 2’s complement.

        tmp = (uint8_t) (offset && 0xFF00) >> 8;

        baro_sensor_write_reg( LPS25H_RPDS_L, tmp );

        tmp = (uint8_t) (offset && 0x00FF);

        baro_sensor_write_reg( LPS25H_RPDS_H, tmp );

    ♯ endif

        return who;

    }

    And fucntion used to get pressure and temperature :

    /**

     * @name get Pressure reg in 1 I2C access

     * @brief pbuf : LPS25HB pressure 3 regs 8-bits values in one buffer

     */

    void pres_lps25h_get_regs_pres(uint8_t *pbuf)

    {

        baro_sensor_read_regs(LPS25H_PRESS_OUT_XL | LPS25HB_I2C_MULTIPLEBYTE_CMD , 3, pbuf );  // LPS25HB_I2C_MULTIPLEBYTE_CMD to get multibyte

    }

    /**

     * @name get Pressure reg in 1 I2C access

     * @brief pbuf : LPS25HB temperature 2 regs 8-bits values in one buffer

     */

    void pres_lps25h_get_regs_temp(uint8_t *pbuf)

    {

        baro_sensor_read_regs(LPS25H_TEMP_OUT_L | LPS25HB_I2C_MULTIPLEBYTE_CMD , 2, pbuf );  // LPS25HB_I2C_MULTIPLEBYTE_CMD to get multibyte

    }

    in the config setup :

    if LPS25HB_FIFO_CTRL is in bypass, both temp and pressure are good

    if LPS25HB_FIFO_CTRL is in LPS25HB_FIFO_FIFO_MEAN | LPS25HB_FIFO_WTM_32, only pressure is okay and temperature is too high.

    Further more, I am not sure that the pressure is really filtered in FIFO_MEAN mode compared to BYPASS mode according to dump value analysis.

    Any idea please ?

    Thanks,