Question
LPS25HBTR pressure reading decreasing over time
I have bought a MKI-165V1 to test LPS25HBTR,but I find that the pressure value is decreasing for a long time ,from 1014.117 to 1002.970 in an hour.It is not stable,the next is my initial code,what is the reason for it
uint8_t data = 0x90;
HAL_I2C_Mem_Write(&hi2c4, 0xB8, 0x20 , I2C_MEMADD_SIZE_8BIT, &data, 1, HAL_MAX_DELAY);
HAL_Delay(10);
data = 0x00;
HAL_I2C_Mem_Write(&hi2c4, 0xB8, 0x21 , I2C_MEMADD_SIZE_8BIT, &data, 1, HAL_MAX_DELAY);
// HAL_Delay(10);
// HAL_I2C_Mem_Write(&hi2c4, 0xB8, 0x22 , I2C_MEMADD_SIZE_8BIT, pData, Size, 0xFF);
HAL_Delay(10);
HAL_I2C_Mem_Write(&hi2c4, 0xB8, 0x23 , I2C_MEMADD_SIZE_8BIT, &data, 1, HAL_MAX_DELAY);
HAL_Delay(10);