lps27hhw problem with negative temperature
Hello
We use the lps27hhw in our devices. When temperature is positive - all right. But when temperature is negative - the sensor sends the temperature less than it actually is (example -40* instead -20*).
I put the appliance in the freezer, the temperature is -19*, and show data from the sensor via BLE app.
0 byte - status reg
1-3 bytes - pressure reg
4-5 bytes - temperature reg
The sensor send -38 degrees of celsius.
After that I put the device in the oven, the temperature is +50*. All right.

What is the problem?