LPS28DFW bias stability / difference with other LPS28DFW
Hi,
I have two LPS28DFW in my application. The absolute value as well as the difference is important here. I noticed that there is a difference of around 30 Pa. Is it reasonable to assume that this difference is roughly constant in the future? I tested it for around 5000 seconds (see attached scatter plot and histogram for the difference) and it was pretty stable (sensor temperature was ~31°C in both cases). I am also going to test it for a longer time period but I'd like to know from a theoretical standpoint if I can assume this to be roughly constant and if I can use this for a "factory calibration" of my application to improve accuracy.
Thanks for your help.