LPS33HW accuracy question
Hello,
I have a question related to accuracy of this sensor see attachment
From the datasheet I can read that the accuracy over temperature is +/2.5hPa. Did I correctly understand that the accuracy of the sensor can change within this range only in this given range of temperatures 0-65C ? But in this case what is the reason to bake in the temperature compensation ?
Second in order to reduce the variation you suggest to run OPC ( one time calibration ) to get better +/- 1hPa accuracy. Could you explain the procedure how this calibration should be done? Any suggestion...
Third question is related to the long time stability which you stating is around +/-1hPa over year. In this case also do you have any recommendation how to address this changes ?
Last observation: all this numbers are connected to 1.8V @ 25C Test conditions. So how this condition are connected with the specified ranges of the temp from 0C to 65C ? Second could you share how input voltage can affect those values ( in my case I am using 3.3V supply instead of 1.8V) ?
Thank you very much in advance
Jacek Pieczaba