LSM303AGR, Accelerometer Read Address cannot be auto-incremented.
Hi, I'm using LSM303AGR.
I cannot read acceleromter 6bytes from 0x28 _ 0x2D.
It is read only 0x28 register 6 times.
I tried to read other register, 0x20 0x21, etc...
Likewise, It is read only first address register 6 times or several times.
I also checked MS bit (bit1). it is 1 of course.
BUT!
It works Magnetometer same way!
I can read 6 registers magnetometer data.
Below Configure values.
- ODR : 1001 (1.344kHz)
- LPen : normal mode
- Zen, Yen, Zen : 1
- BDU : 0
- BLE : 0
- FS : 10 (8g)
- HR : 1
- ST : 00
- SPI_ENABLE : 1 (3 wire)
Below, my configuration code and reading code
Sensor_IO_SPI_CS_Enable(&SensorHandle[ACCEL]);
valueTx = 0x29; //8g(Sensitivity : 3.9 mG/LSB), HR mode, 3 wire
Sensor_IO_SPI_Write(&SensorHandle[ACCEL],LSM303AGR_ACC_CTRL_REG4,&valueTx,1);
Sensor_IO_SPI_CS_Disable(&SensorHandle[ACCEL]);
Sensor_IO_SPI_CS_Enable(&SensorHandle[ACCEL]);
valueTx = 0x97; //1.344kHz, no power down(12bit, divisor : 16), x,y,z enabled
Sensor_IO_SPI_Write(&SensorHandle[ACCEL],LSM303AGR_ACC_CTRL_REG1,&valueTx,1);
Sensor_IO_SPI_CS_Disable(&SensorHandle[ACCEL]); Sensor_IO_SPI_CS_Enable(ctx);
Sensor_IO_SPI_Read(ctx,ctx->RegRX, raw_data_tmp.u8bit,6);
Sensor_IO_SPI_CS_Disable(ctx);