Skip to main content
Visitor II
September 2, 2025
Question

LSM303AGR Application Note Clarification Needed

  • September 2, 2025
  • 1 reply
  • 560 views

Hello everyone,

I am currently using the LSM303AGR's magnetometer and accelerometer. After coding the self-test procedure from the datasheet, and noticed that the number of samples for the magnetometer self-test is way higher than the number of samples for the accelerometer self-test (5 for the Accelerometer, 50 for the Magnetometer).

When looking at the Application Note (AN4825: ultra-compact high-performance eCompass module based on the LSM303AGR), the number of samples to average is 5 at page 21/65 - Magnetometer self-test), whereas it is 50 in the next figure at page 22/65 (Figure 3. Magnetometer self-test procedure).

Which one should it be ?

Thanks in advance,

CJ

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    September 11, 2025

    Hi @jasoncerisier ,

    Thanks for notice us.

    Let me check with the team and come back to you.