Skip to main content
Visitor II
March 5, 2019
Question

LSM303AGR CTRL_REG4 FS[1:0] Full Scale Selection is reversed?

  • March 5, 2019
  • 0 replies
  • 406 views

Hi,

Based from the LSM303AGR CTRL_REG4 FS[1:0} Full Scale Selection are (00: ±2g; 01: ±4g; 10: ±8g; 11: ±16g).

I tried all settings and it is reversed. So, setting 00 is +-16g. So is this an error in the datasheet?

Regards,

Markel

    This topic has been closed for replies.