Skip to main content
Explorer
July 4, 2014
Question

LSM303D temperature format

  • July 4, 2014
  • 2 replies
  • 620 views
Posted on July 04, 2014 at 15:19

Hello,

I got good results reading accelerometer data but the temperature register is about 36 (decimal), the datasheet mentions 8LSB/°C, 36/8 = 4.5°C, this is quite cold ;)

Room temp is 24°C, the other sensors located near the LSM are indicating 28°C.

What is the good conversion factor?
    This topic has been closed for replies.

    2 replies

    Visitor II
    July 14, 2016
    Posted on July 14, 2016 at 03:09

    Hi,

    I see there has been no replies to your post for the past 2 years.

    Check out this disappointing answer by Miroslav from ST:

    /71915817

    ST Employee
    August 12, 2016
    Posted on August 12, 2016 at 09:27

    Unfortunately

     the temperature sensor can be used only to measure temperature variations. It isn't suitable to return absolute temperatures measures. The value represents difference respect to a reference not specified value.

    Best regards

    Miroslav