Skip to main content
Visitor II
March 23, 2015
Question

LSM303D Z-axis Direction

  • March 23, 2015
  • 0 replies
  • 545 views
Posted on March 23, 2015 at 23:28

Why if the LSM303D a steady-state on a horizontal surface measures 0 g on the X-axis and 0 g on the Y-axis, whereas the Z-axis measures 1g = 1000mg?

Direction of  Z detectable accelerations is upward (see pag. 8/52 DocID023312 Rev 2 DM00057547), this would imply that the Z-axis should measure -1g = -1000mg

#lsm303d #z-axis #accelerations
    This topic has been closed for replies.