Question
LSM330DLC data sheet questions
Posted on November 07, 2013 at 19:32
Hello,
I need to configure a LSM330DLC in a way outlined in the DT0005 document. Essentially, on data ready interrupts (INT1_A) from the accelerometer feed into the DEN_G pin, telling the gyro to push a conversion onto the gyro FIFO. In this way, acceleration and gyro data are aligned (I think). In addition, I want to have a FIFO watermark interrupt as well as an interrupt to wake my board up upon movement. I believe I need to setup three interrupts sources: 1) INT1_A to be I1_DRDY1 (or is it I1_DRDY2?) Which one does what? 2) INT2_A to fire upon a motion detection event. I believe I see how to do this with INT1_A, but I need it to happen on INT2_A. 3) A FIFO watermark interrupt to fire from the gyro side (INT2_G). This one I have figured out, but need INT1_A/DEN_G working before I can fully test it. More to the point- 1) In table 18, there are INT2_CFG_A, SOURCE_A, etc registers, but I see no mention of them in the section 8 description. Does anyone know how to configure INT2 on the accelerometer. 2) What is the difference between DRDY1 and DRDY2? (See table 26). In short, how do I make INT1_A fire upon every accel conversion? 3) The text after table 43 ''The content of this register is loaded at boot?'' OK, so if I want to change it do I need to reboot for the changes to take place? I also do not see in table 18 which registers are actually loaded at boot. 4) If I am doing it properly, rebooting does not appear to wipe out FIFO count. Is this the correct behavior. 5) What does Figure 20 mean? Thank you in advance for your help, Shane #lsm330dlc-drdy-interrupt #lsm330-lsm330dlc