Skip to main content
Visitor II
February 25, 2016
Question

LSM6DS3 gyro data is off by about 15% of what I expect

  • February 25, 2016
  • 1 reply
  • 817 views
Posted on February 25, 2016 at 19:26

Greetings.

I am trying to get accurate gyro data out of the LSM6DS3, but my results are about 15% off of what I expect.

 

My test setup is a PASCO scientific Rotary Motion Sensor (RMS) with a LSM6DS3 mounted on top of it.

I configured the LSM6DS3 such that full scale +/-32767 is mapped to +/- 1000 dps.

I then rotated the RMS and LSM6DS3 at 366 dps (as measured from the RMS) and the LSM6DS3 gyro reported a z-axis rotational value of 10173.

My calculated gyro z-axis rotational velocity for this value is

10173 counts * (1000 dps / 32767 counts) = 310 dps.

Why is the gyro reporting 310 dps when it is being rotated at 366 dps?

What is the guaranteed accuracy of the gyro?

Thank you

Scott Wild

    This topic has been closed for replies.

    1 reply

    Visitor II
    March 17, 2016
    Posted on March 17, 2016 at 15:19

    Hi Scott,

    The actual value of one ADC count at your setting is 35 mdps, according to the datasheet. If you use this value, you will get a much closer result. I suppose they call the full scale +-1000dps just to give it a round number. The actual full scale would be 0.035*32768 = 1147 dps.